Other Parts Discussed in Thread: MRD2EVM
Hi All....
Referring to the original locked thread, I'm having the same problems identifying a usable antenna for a new smart tag design. With all due respect to TI, I would appreciate knowing the reasoning for effectively dropping support for this product! The ez430-TMS37157 is flat out NOT available anywhere (China sources are all SCAMS!), The READER in the eval kit shows up on the TI store as RI-ACC-ADR2-10 for $199. I just confirmed that it will be in stock in sometime in September, but it does not have the smart tag in the kit....so I am designing a replacement using an MSP430FR5994IRGZ chip rather than the -2744. This may be available for sale by me at some point (kborsum@dascor.com). Also, the MRD2EVM reader kit is available from Mouser for $70 or so, and appears to support the same functionality, but without the big air coil.
I had a long chat with Allan Burk (sp?) at ECIworld.com this afternoon, and he confirmed that all of the Neosid antennas are special order, and that Neosid probably doesn't stock them either--and he implied that Neosid really builds everything to order, so there may not be anything "in inventory." ECI does have a 3-axis part A3D4-2506 listed as stock, and the three axes in parallel work out to abut 2.48 mH....so this might be a usable solution--and give you three-axis support as well. I'm still waiting on price and availability from ECI, and from Neosid in Germany as well.
Again, referring back to the original thread, the last post mentioned that he had reworked the design for a different inductance and capacitor. It was indicated that the tuning range for the capacitor in the TMS was 30uF....so I would like to confirm that the external cap should allow for a 15 uF internal cap in parallel with the external cap to allow maximum adjustment range? Discussion please!
Finally, if anyone out there has successfully implemented a design using parts from Coilcraft, or Toko, I'd sure appreciate your input. Particularly specific part numbers and capacitance values used.