Hi All:
I have some questions needed to be checked.
1. Does following figure means the first time power on ?
2. After power on, if implement EN reset and EN lead than SS about 1ms (Nevertheless SPI have been set at the first power on).
Dose there have some risk due to violation of Figure's rule?
** MOSI/MISO/CLK are directly connected to MCU, 7970 SS is connected through some logic gate to MCU.
3. Does there has any constraint for EN pin (Rising time, falling time etc..) ?
Thanks !