Other Parts Discussed in Thread: CC2500, CC2650, CC1310
Hi,
I would like to use CC1350 for BLE and proprietary 2.4GHz communications.
Currently I'm using the CC2500 for the proprietary with MSK modulation, and would like to do the same with the CC1350.
In addition, I also would like to have a subG network as well, so that the CC1350 will have BLE, and 2.4GHz and subG propriatry networks.
Is that possible?
Thanks, Isak.