Hi All,
After I understood that TI cc1350 does not support the BLE and sub1-ghz at the same time, and the only option for now is to set dual image, i have few questions about dual image:
1- Did the cc1350 came with more than 128KB?
2- Did 128KB is enufh to run BLE and sub1-GHz?
3- Did there is any example to run dual imag?
4- In the dual image the moving from BLE and sub1-GHz done by hardware interrupt, can i replace this interrupt in timer interrupt, like each 10 seconds i change from BLE to sub1-GHz and Sub1-GHz to BLE?
5- Did there is a way to share memory between the SUB1-GHz image and the BLE and the boot-loader? example: if the BLE connected i want to disable the SUB1-GHz, so i need update some flag, and the interrupt timer (that suppose to replace BLE to sub1-GHz) will read this value and do not replace the BLE.