Using CC2650 pg-2.3. Using TI-RTOS / SimpleLink 2.11. Using IEEE 802.15.4 mode.
I need to enable Continuous Wave mode for factory testing.
I have verified that our proprietary designed board works okay, using SmartRF Studio 7.
In my code, I have issued the CMD_RADIO_SETUP, CMD_FS, and CMD_TX_IEEE radio commands.
They report a successful start (DONE_OK, DONE_OK, ACTIVE), but I do not get any output signal.
The external 24 MHz XTAL is running okay.
The first lines of code in my main() function are:
HWREG(PRCM_BASE + PRCM_O_RFCMODESEL) = PRCM_RFCMODESEL_CURR_MODE2;
SysCtrlPowerEverything(); // Power up all chip peripheral modules.
Power_setConstraint(Power_SB_DISALLOW); // Do not allow the chip to power down.
Are additional actions required?
Is there an example of how to enable the Continuous Wave mode? I need modulated and unmodulated variants.