Hello TI-Forum,
i have several questions regarding the CC2650 Proprietary Radio. I have the proprietary protocol running with the settings from the "Packet TX / RX" Examples.
I wanted to change the baudrate and so i have several questions regarding this:
- the smartf_settings.c says in the comments at the top that the symbol rate is 50 kBaud. However when applying the formula form the hardware reference manual i get 200 kBaud
- R= 131072, p = 15, f_clk = 24000000
- (131072 * 24000000) / (15 * 1048576) = 200000
- So did i make a mistake, or is the comment wrong?
- I changed the .rateWord to 262144, to double the baudrate. I did that both in the transmitter and the receiver. However the receiver simply does not receive anything at all. Is there something else i have to do?
- I have read at different places in the forum, that settings for 1, 2 and 5 MBaud are available. How can i obtain them?
- I would have tried to obtain this information via smartrf-studio7 (v 2.6.0), but it does not seem to contain settings for the CC2650 propriatary radio mode. When will this be available?
- What can i do in general, besides keeping the frequency synthesizer running and disableing the inactivity timeout, to speed up the sending process and minimize the send-delay?
Thank you in advance
regards