Tool/software: Starterware
Hi..
I have a sensor tag cc2650 , one more cc2650 radio module that supports zigbee, 6lowpan, ble, etc..
and a PHYGATE ,ARM335x gateway.
I want to implement a IoT system for reading the sensor data and sending it to the cloud with the following requirements:
Read the Sensor Data using :
1. BLE
2. 6LOWPAN
3. Zigbee
4. Lora
Send the same info to the cloud using:
1. MQTT
2. LoRA
3. Zigbee
4. 6Lowpan
As per my understanding, I need to have three programs in hand :
1. Code for reading the data received by cc2650 (Some cases, another cc2650 module is connected to the gateway to receive the data from sensortag)
2. Programs for BLE, 6LOWPAN, Zigbee, Lora for sending the sensor data on the sensortag side
3.Program for initializing MQTT, LoRA, Zigbee, 6Lowpan protocols inorder to establish the connection with tag and reading the data and sending it to the command prompt//screen on the gateway side.
Can any one help me in implemmenting this with necessary docs and codes available?