For my appllication I need the max. capacity i.e. 4 slaves connected to a Master with 44,1k PCM bandwidth. In this setup I have got a problem with one pf the slaves losing connection with the master and then reconnecting after a dozen or few tens of seconds. I actually use a PPath binary generated with a possibly bit old version of PP-CFG, of over a year ago. Has such a problem been spotted by TI support in the meantime and there is a chance it has been corrected in the current PP Configurator ?
If not, since I can imagine this behaviour can possibly be due to varous reasons what kind of information should I collect to effectively diagnose this issue ?
Regards, Pawel