Other Parts Discussed in Thread: TIMAC,
Hello,
I’m using TIMAC 1.5.2 on CC2650. I would like to perform a transmitter test using the Transmitter Test Command (CMD_TX_TEST) in my application.
- First, I want to set the Transceiver in send mode, by using the CMD_RADIO_SETUP command, to set the following parameters:
mode = 0x02 (IEEE 802.15.4)
txMode = +5bBm
2. Second, I want to execute the CMD_TX_TEST with the following parameters:
config.bUseCw = 0; // Send modulated signal
config.bFsOff = 1; // Turn frequency synthesizer off after cmd
config.whitenMode = 1; // Default whitening
txWord = 0xAAAA; // Value to send to the modem before whitening
syncWord = 0x71764129; // Sync word to use for transmitter
endTime = 0; // Time to end the operation
Can someone tell me, how can I implement this RF Core commands in my application (using possibly existing TIMAC routines)?
Thank you for your help,
Rachenka