This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC2520-CC2591EM_RD: PCB Layout File

Part Number: CC2520-CC2591EM_RD

What is the PCB tool in which, the "CC2520-CC2591EM.pcb" was designed? Which tool can be used to open/view the same for reference ? I tried to view the same using Pads Layout Viewer VX.2.1 but was not possible open

  • The design was done using CadStar. You can use any gerber viewer to import the gerber files and look at the design. There is also a CadStar Express, which is freeware, that can be used to import the PCB and SCM files if the design is not too big (number of nodes). Not sure if this particular design van be imported into CadStar Express or not.