Other Parts Discussed in Thread: TIMAC,
Tool/software: TI-RTOS
Hello All,
I am currently working on TIMAC - Power management module for cc2650
IAR Workbench version - 7.40.2.8570, TIMAC - 1.5.2, TIRTOS - 2.11.01.09(For SimpleLink Wireless cc 26xx MCUs this is the latest version).
Once MAC_RX_ON_WHEN_IDLE is set to FALSE, the CPU is not coming out from sleep mode.
Analysis done :
1. 24Mhz stops clocking (expected in the sleep mode).
2. 32Khz also stops clocking(Not expected)
The above issue is not observed in the development board that uses CC2650EMK-7ID (7x7 Package).
The issue is only observed on our custom board that uses CC2650-4XS (4x4 Package).
Note: The issue is not present once the target CC2650-4XS is in debug mode.
Please help
Thanks
Naveen