Hi TI Team,
We are connecting a device to the host MCU(CC2650F128RHB).The device datasheet says that it can support max 160K bps. So does CC2650 supports SPI interface bit rate of 160K bps.
Can we able to transmit and receive at 160Kbps from CC2650. The datasheet of CC2650 mentions that "The SSIs support both SPI master and slave up to 4 MHz" but it doesn't tell us about the lowest frequency up to which it can support serial communication.