This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LAUNCHXL-CC1352R1: Bad sensitivity

Part Number: LAUNCHXL-CC1352R1
Other Parts Discussed in Thread: CC2650, , CC1352R

I'm trying to verify the RX performance for the CC1352 for 802.15.4 at 2.4GHz.

I'm using one device as the TX and another device as the RX (DUT). Between the two devices is a variable attenuator. The DUT is in a shielded box.

For the TX, it is setup to send 20 octet packets at +5 dBm. By the time the signal gets to the RX side it is +3 dBm (when the attenuator is set to 0 dB). This was verified with a spectrum analyzer.

The attenuator is then adjusted until the PER is greater than 1%. At that point the RX sensitivity level is calculated by taking the RX power received with no attenuation (+3 dBm) and substracting the attenuator value when PER is greater than 1%. In this case the attenuator is 90 dB, thus the sensitivity level is (+3 dBm - 90 dB = -87 dBm). The data sheet states it should be -101 dBm.

To check the setup I've also made the same measurement on CC2650 board. The level is -100 dBm for PER of 1%. It matches the specification in the datasheet.

I can't imagine the CC1352 sensitivity level is so far off from the datasheet (-87 dBm measured vs -101 dBm stated in the datasheet).

Any suggestions to what is wrong or something to check?

For the DUT I'm connected to SMA contact, J7

The LaunchXL-CC1352R1 board does have an RF switch to route either the 1GHz or the 2.4GHz to the antenna. I haven't measured the control signal, but maybe it is not enabled for 2.4 GHz.

Please let me know.

Michael