Other Parts Discussed in Thread: CC2650MODA, CC2650
The CC2652 and CC2650 pin outs are identical. Does that mean the launchpads are identical apart from the chip on the board. So if I changed the CC2652 chip on the launchpad to a CC2650 chip would it becomme the same as a CC2650 launchpad. Further if I change the CC2650 chip on the CC2650MODA, to a CC2652 chip would it function correctly. I suspect it would not because of some operational code contained in a ROM on the CC2650MODA module. Can someone confirm this?
Is there a plan to release a CC2652MODA module, similar to the CC2650MODA?
Cheers.
Mark.