Hello,
I activated the auto-ack functionality by setting the bit "autoAckEn" to 1 (and "slottedAckEn" to 0 ) but it's not working as I expect.
Indeed, it seems that no ack are sent by my CC1352R even if correct data frames are received (and conditions described in section 25.5.4.1.3. of the datasheet are met)
For example :
I received 10 correct RxData frames in my radio buffer and in the output field of the IEEE Rx commands the counter "nRxData" is equal to 10
But the "nTxAck" counter is equal to 0 (should be equal to 10 ?) and I don't see any "ACK" on my sniffer.
Is there something missing in my configuration (in addition to "autoAckEn" bit)?
Thank you for your help
Environment
LAUNCHXL-CC1352R1
sdk 2.10.00.48