This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC1352R: Run radio command before bios start

Part Number: CC1352R

Hello,

I'd like to know if it is possible to run Tx or Rx radio commands before starting Bios ?

Indeed, it seems that Rx or Tx commands sent before runtime do not work (and "RF_runCmd" generates an exception).

I need to implement an OTA update which works without scheduler.

Thank you for your help

Environment

LAUNCHXL-CC1352R1

sdk 2.10.00.48

2.4Ghz IEEE 802.15.4