Other Parts Discussed in Thread: CC2592, BQ25015
Hi,
My design is using the CC8520 + CC2592 on both the protocol master and slave. Peak radiated power measurements for master and slave are both around +20dBm. However, I only see about 40ft of line-of-sight range in a practical test, beyond which RSSI falls to <-70dBm and audio cuts out.
Furthermore, in a conducted-to-conducted test where the master and slave are connected together through coaxial connectors and attenuators, the connection is maintained. I was able to put 110dB between the master and slave and maintain the connection. This seems like the correct performance based on the link budget calculation, 20dBm - 110dB + 11dB LNA gain = -79dBm. Sensitivity of -87dBm per the datasheet confirms the connection is expected to be maintained.
I just can't figure out why I'd lose RSSI so quickly in an over the air test if the radiated power is +20dBm and the receivers are working at -79dBm. Multipath? Interference in the environment? Anything I can debug with the test commands?
Thanks,
Arthur