Need to implement internal flash OAD function on 2.4GHz proprietary. Since there is no existing example, current idea is that refer to rfWsnNodeIntFlashOadClient and rfWsnConcentratorOadServer in CC13x0 SDK 1.60.00.21, implement application level code, and directly using bim_onchip under C:\ti\simplelink_cc2640r2_sdk_2_20_00_49\examples\rtos\CC2640R2_LAUNCHXL\blestack\simple_peripheral_oad_onchip\tirtos\iar\bim_onchip for BIM part.
Is it on the right direction? Is there any modification needed for BIM?