Hi,
I'm using CC1110 and need to stay in PM2 about 30-100ms. This is not a problem, so datasheet says it shoud be larger than 11ms.
But, what I need is stay only 30us in active mode.
I'm using Simpliciti and this code:
while(1)
{
event = BSP_SleepFor( POWER_MODE_2, SLEEP_1_MS_RESOLUTION , 30);
BSP_TURN_ON_LED2();
}
Inside BSP_SleepFor(), I turn off led before bsp_PowerMode():
BSP_TURN_OFF_LED2();
bsp_PowerMode(mode);
What I get is 30ms with led in OFF state. This part is OK.
But the minimum time I get with led in ON state is 2,5ms. I need 30us.
is it normal spend this time only to go to PM2 mode?? is it possible reduce this time to 30us?
Thanks.