Eventually the CC1310 will support fast data rates (~4.4Mbps), however, the UART is capped at 3 Mbps.
As part of my design I would like to route serial data to and from the CC1310 as fast as possible, preferably at/above the max data rate available by the CC1310.
- Is it possible to do this with an existing communication interface in the CC1310?
- If not, would it be possible to route data using interrupts to GPIO pins? Then, I could communicate to an "interpreting" MCU and then to UART. Although, the extra latency may not make it worthwhile.
Thank you!