Hi,
I would like to use CC1310 in the design, the transmitter uses other vendor equipment, the receiver uses CC1310.
Modulation mode using OOK. The transport protocol uses a custom protocol,
and the logic 0 and 1 of the transport data are defined using custom methods (with the duration of the level).
Now the debugging will be encountered such a problem:
Directly using the settings in the SmartStudio can not properly receive the transfer data.
The current phase of the target:
I want to directly read out the data which the Radio side convert modulated signals into bits.
(The data is before the RFcore decoding, and including all the Preamble, Sync word)
There are the following questions to help.
How to set the CC1310, in order to all the RF side of the comparator data into the reg or a bit, easy to read when debugging.
Thank you
Jacky