My application is a sensor node:
- Sends tx data once a 5 minutes
- Is in RX mode the rest of the time
What works:
- Send tx data once a 5 minutes
or
- Receive data from interrupt
What does not work:
- Be in receive mode -> EasyLink abort -> send something
What I try to do:
- Be in receive mode -> switch to send mode -> send something -> be in receive mode.
Application is almost done and ready for customer but I can't seem to get this to work.
It always fails when doing EasyLink abort with various 'status errors' depending on what I try.
If at all possible It would be best If a TI employee could make a really simple example that:
Sends something -> goes in rx mode -> sends something ....
using the EasyLink 'driver' .
Using the node example requires a complete code overhaul since it does not use the Easylink Driver.
My used functions and some parts of the code can be found here:
I appreciate any help. Need to get this done ASAP