Hello,
I am using the sample examples of TI-RTOS on smart RF boards+cc13xx.
I have successfully seen the working of Tx/Rx example given.
Its written the code is working at Symbol Rate: 50.00000 kBaud
I want to change it to 100kbaud.
I want to do the changes in the code and not in smartrf studio as given
Its wriiten changes has to made in the smartrf_setting .c file of tx/rx
these are the two parameters which are with respect to symbol rate in the file
.symbolRate.preScale = 0xf,
.symbolRate.rateWord = 0x8000,
i am not able to decode how they represent 50kbaud..
what changes should i make for 100kbaud
thanks