hello,
I have tested the TI-Rtos Tx/Rx code for smartrf +cc1310 boards and tested using the samrtrf studio .its working fine.
now i want to do the data transmission with and wi-sun stack based on ieee 802.15.4g on another board.
since both are running on ieee 802.15.4 standard data transfer should be possible .is it .
i have kept in mind the channel used symbol rate,transmission power .
but when its comes to packet frame i am quite not sure what field should be same .i have kept the preamble size and sync word size in both stacks same.
but still packet transfer is not occurring.
please do help.
thanks