Hi,
Our customers are thinking of the measurement of RSSI.
Since there are some necessary information, please let me know.
#1
Figure 3-12 of the data sheet P.40 is a typical, could you provide MIN and MAX value?
#2
In the RSSI accuracy of RSSI Section Characteristics of data sheet P.11, there is a only typical value at 310MHz.
Could you provide MIN, MAX value and the data at 125 deg?
If possible, I want also data of 433MHz.
#3
Could you provide the measurement data of the actual value of the above RSSI variation?
#4
TX to RX switch and RX to TX swirch in datasheet p.16have been described only TYP value,
could you provide the minimum and maximum value?
Best regards,
Tomoaki Yoshida