I want to get it to work on 433MHz. The datasheet say: "The design can easily be adapted to other frequencies such as 169 MHz, 433 MHz, 868/915/920 MHz."
What should I do to adopted design on 433MHz???
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
For 14 dBm output power, the standard ref design can be used. The Chinese AMR Reference design can be used for different frequencies only if a higher output power is needed. i.e. > 20 dBm.
//Richard
Extra filtering was required for the 490 MHz design. For the 868 MHz design, the harmonics were at a sufficient level so a 0 ohm resistor could be used. If extra margin would be required for the harmonics then an inductor can be used for filtering purposes.
Hi Taka,
This design can also be used at 868 / 915 MHz as well but I recommend to look at the CC1190 as a first choice of FEM since this contains a PA, LNA and switch.
Please refer to the standard schematic for the discrete PA design (v.1.3.6) for the standard BOM for 490 MHz. To update the design to 868/915 MHz, please update the following values:
L21: 5.6 nH
L22: 0 ohm
C21: 8.2 pF
C22: 2.2 pF
C23: 120 pF
R21: 15k
R22: 3.9k
L23: 12nH
L24, L25: 1.8 nH
C24: 5.1 pF
C27: 3.9 pF
C28: 3.5 pF
C29: 3.9pF
Expect around 20 dBm with this BOM for 868/915 MHz but the values are dependent on the layout.
Regards,
Richard