I have some problems using the libraries for the I2C
Are the i2c libraries complete or not?
I saw that in i2c_open() function there is a control on the first parameter (index).
If it is greater than i2c _count= -1 the function return NULL. I don't understand this control because the unsigned int "index" is used as index in a vector (i2c_config vector).
Where i can fill i2c_confing vector? and why i2c_count is equal to -1?
Simone Trinchero