Hello,
I would like to know when the MAC2.0 will be available?
I would like to use it before the end of july, I hope to get it before.
Best regards,
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello,
I would like to know when the MAC2.0 will be available?
I would like to use it before the end of july, I hope to get it before.
Best regards,
Hi Ronie,
Do I understand correctly that when I add IEEE 802.15.4g stack in SmartRF Studio for my configuration it automatically adds FHSS support?
Igor
Hi YiKai,
As far as I understand rfWsnConcetrator & rfWsnNode examples do not include FHSS. Am I wrong?
At least, when I want to generate smartrf_settings file set, by default it does not have whitening feature, however there are several sets for using IEEE 802.15.4g
I have downloaded and installed that SDK, but when open according .h & .c files I do not see any visible changes comparing with the previous versions. Where in that project can I see information about such support?
Thanks,
Igor
So, how to add FHSS to the example?
Are there any other examples that could be used for communication test with FHSS?
Igor,
It is actually pretty complicated to implement a well functioning frequency hopping system, this is why we implemented a open standard solution based on 802.15.4g standards.
We do actually have a nice little stack called SimpliciTI, which shows how to implement a frequency hopping solution and we have released it open source :
Regards,
/TA