Hello,
We are considering CC1350 to replace CC2640 in our project.
Our Current Topology is based on 2 CC2640 devices acting as peripheral/central BLE.
The bellow 2 options were raised:
1. Keep current topology, utilize CC1350 as single band 2.4Ghz:
CC1350 acting as peripheral BLE.
CC1350 acting as Central BLE.
As i understand, Range would be improved as CC1350 outputs 9db, as opposed to cc2640 5db (please approve).
2. Communication between the nodes in Sub-1Ghz, and both nodes act also as peripheral BLE:
CC1350 acting as peripheral BLE (for Mobile phone connectivity) + tx/rx in Sub-1Ghz to communicate with second node
CC1350 acting as peripheral BLE (for Mobile phone connectivity) + tx/rx in Sub-1Ghz to communicate with second node
Is this solution feasible?
in the Ti-RTOS 2.2.0 example (rfWsnDmNode/rfWsnDmConcentrator) the 2.4Ghz is used as broadcaster, and doesn't establish a BLE connection.
If such solution is feasible, is there any example available?
Thanks,
yuval.