Hi,
I'm using a cc1310 custom board.
I have seen the WOR RX example code. It run a RX_sniff command right? Once it runs, then the RF core will be in the RX sniff state after a while which the time has been set in the "RF_cmdPropRxSniff.startTime" . After the RX sniff working period, it gives a "RF_EventLastCmdDone" message in the callback. Is that right?
I replant the code to my custom board. There are the peripherals i used : UART, GPIO, PIN interrupt, and RF core.
I want to ask, can i just leaving the RF core,just let it restart the period automatically ? If i have to restart the period, then the power of the hole device is too high (it's about 1.5mA on my board, no such things like LED and i disconnected the XDS debugger). I think the TI-RTOS just put the device into wfi state. But what i want is that it could stay in the standby state. Once there is any data received from the RF core. It wakes up the main core and the main core does the relevant response.
I think it should be around 7uA when the device is at sleep period of RX sniff state. And should i close the UART before entering the RX sniff state?
Hope you could help me , thanks.
BR,
Mikel