Our current system is based on the CC1100 / CC1101 in MSK mode (250000 + FEC, MSK).
The task - to use the same system transceivers CC1200.
I tried to use a 2-FSK modes, 2-GMSK a deviation of 62.5 kHz, 127 kHz - CC1101 does not accept packages from the CC1200.
When I tried to pass on to the CC1200 CC1101 in any combination 2FSK & 2GFSK - packets are transmitted normally, therefore, the other settings are correct transceiver.
However, to send a packet to CC1101 mode MSK I still can not.
1. The problem generally solved in principle?
2. If yes - then how do I configure the CC1200 configuration for such a mode?