I just received two CC1310 Launchpad development boards. I want to use the on-board option for external antenna. Looking at the schematic I see that the RF connector chosen is a Murata MM5829-2700. I have spent the last 2 days trying to find a mating cable for this part, one with a mating JSC connector on one end and an SMA connector on the other so that I can connect an external dipole antenna. So far, no luck.
Questions:
1) Why was this particular connector chosen when there is so little support for it? Standard U.FL connectors are readily available and roughly the same price. They are supported by many mfg and mating cables are easy to find.
2) Do you have a particular mating cable in mind for this interface? If so, please share the details regarding part numbers and suppliers.
3) Can this connector be replaced by U.FL connector with a reasonable chance of success?