I use CC1310 LP together with the booster pack sharp display. TIRTOS mw for the display works well.
It stops working after having implemented SPI functions to work with the on-board external flash memory. The display handle does not initialise any more (Display_open) after previous SPI operation to read/write the external flash. I think the previous SPI operation is correctly terminated by using the bspSpiClose function. The spiHandle becomes uninitialised.
By the way. In difference to the SPI handle the LCD handle (hDisplayLcd) stays initialised after having closed the session (Display_close). This indicates a different implementation in the firmware stack and maybe to a permanent allocation of the SPI bus.