Hello,
Do CC1120 and CC1200 have any possibility to apply to the ARIB STD-T98 system?
In case modulation format is 4-FSK, CC1120 and CC1200 may apply to the ARIB STD-T98 system, I think.
Best Regards,
Nomoto
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello,
Thank you for your reply.
ARIB STD-T98 is needed a radio station license and is for mobile object.
Some of specifications are following:
Frequency: 467MHz (from 467MHz to 467.4MHz)
The number of channels: 65
Modulation format: 4-FSK (+/-945Hz, +/-315Hz)
Channel space: 6.25kHz
Data rate: 4.8kbps
Allowable deviation of frequency: +/-1.5ppm
Allowable deviation of antenna power: +20% / -50%
Allowable deviation of data rate: +/-5ppm
Modulation accuracy (FSK error): lower than 10%
Adjacent channel selectivity: 42dB
Alternate channel selectivity: 53dB
Best Regards,
Nomoto