I need a refresher on how the "Code Export" works with SmartRF Studio, so as to test various RF parameters and modulation schemes.
There are 3 selections in the EasyLink_init() modulations; 50bps2GFSK, 625bpsLRM, & Custom. Am I to assume the command arrays for the first two comes from the file \Easylink\smartrf_settings_predefined.*, and that if I use Custom the commands come from \smartrf_settings\smartrf_settings.*
I have a custom project that is based on the simple Easylink TX/RX examples and want to try various modulations for performance. When I select the modulation as 50bps2gfsk the project works fine. When I export a flavor of LRM (not 625bps) and call the files "smartrf_settings.*" and select Custom modulation, the prject does not work.
Any help would be appreciated.