Hello,
I have loaded simple link RX in launchpad 1 and TX in launchpad 2.
How can I monitor reception of packet in launchpad 2 ?
When I try to turn on SmartRF Studio it tells me I have to update firmware ?! What I am doing wrong ?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
When it says, you have to Upgrade the Firmware then Click on the Upgrade Button then it will automatically do the upgrade and afterwards it recognizes the chip as CC1310. Double Click on CC1310 and it opens up Control panel window.
First you can try the link (TX--> Rx) with SmartRF Studio.
Check RF Parameters Button in SmartRF Studio.
Put one Module in Tx ( Packet Tx), Check Packet count to Infinite mode . By default it loads with 50KBPS data rate at 868MHz. If you want you can change the freq to 915MHz for example. Press Start button
Put the other module in Rx (Packet Rx), make sure Freq is the same as with the Tx freq and press Start button. You should see Receive packets in the Window.
Thanks,
PM
Hello
Thank you for your answer.
I success to use SMART RF Studio for sending packet and receiving using the continuous mode. Now what I am trying to do is to send a triggering sgnal from TX to RX so RX can generate an interrupt at reception of this signal.
How would you process to perform this and how can I monitor this ?
Thanks in advance for your time.
Regards
Hi TER,
My hardware is designed with CC1310 chipset based on sensor tag reference .infact we used same hardware for cc1310 and cc2650. The antenna we used is same as sensor tag pcb antenna .
Btw , what is mean by conducted tests ts ?
Can you plz provide me some info on it .