Hi,
Is there any spectrum measurements available that we could use as a guide line to choose the channel spacing in 1Mbps mode?
In the provided examples the base band filter is set to 0x81. This is reserved value and the comments mention bandwidth of 2.8MHz which sounds very high for this modulation.
Thanks
rfc_CMD_PROP_RADIO_DIV_SETUP_t RF_cmdPropRadioDivSetup =
{
.commandNo = 0x3807,
.status = 0x0000,
.pNextOp = 0, /*INSERT APPLICABLE POINTER: (uint8_t*)&xxx */
.startTime = 0x00000000,
.startTrigger.triggerType = 0x0,
.startTrigger.bEnaCmd = 0x0,
.startTrigger.triggerNo = 0x0,
.startTrigger.pastTrig = 0x0,
.condition.rule = 0x1,
.condition.nSkip = 0x0,
.modulation.modType = 0x1,
.modulation.deviation = 0x3E8,
.symbolRate.preScale = 0xC,
.symbolRate.rateWord = 0x80000,
.rxBw = 0x81,//2.8 MHz 1 Mbps/BLE PHY need this for 868 MHz and Divider5
.preamConf.nPreamBytes = 0x4,
.preamConf.preamMode = 0x0,
.formatConf.nSwBits = 0x20,
.formatConf.bBitReversal = 0x0,
.formatConf.bMsbFirst = 0x1,
.formatConf.fecMode = 0x0,
.formatConf.whitenMode = 0x1,
.config.frontEndMode = 0x0,
.config.biasMode = 0x1,
.config.bNoFsPowerUp = 0x0,
.txPower = 0xa73f,
.pRegOverride = pOverrides,
.centerFreq = 0x0364,
.intFreq = 0x8000,
.loDivider = 0x05,
};