I'm attempting to create a TI-RTOS project for a cc1310F32 or cc1310F64, but I am having difficulty? In CSS, when cc1310F128 is selected as the target, there are TI-RTOS templates, but with cc1310F32 or cc1310F64 selected, there are no TI-RTOS templates. See screenshots below. Is there something else I need to install?
I've asked a similar question on the TI-RTOS forum and was told that TI-RTOS is only officially supported on cc1310F128, not on the 32 kB and 64 kB versions, but based on my searching through the forums, it appears others have put TI-RTOS on the 32 kB and 64 kB versions. Plus, it seems using TI-RTOS is almost a fundamental requirement for using the cc1310.
System details:
Windows 10
CCS 6.2.0.00050
TI-RTOS 2.20.00.06 downloaded from website, not App Center
cc1310F128 has TI-RTOS options:
cc1310F32 or cc1310F64 do not have TI-RTOS option: