TI is excited to announce the release of TI 15.4-Stack v2.0.1! This maintenance release of TI 15.4-Stack is a part of the new SimpleLink CC13x0 SDK v1.0.0. The SimpleLink CC13x0 SDK is a new paradigm of how TI will be releasing software, giving you the developer access to TI-RTOS, examples, and tools needed to develop products on TI’s Ultra Low Power SimpleLink CC13x0 wireless MCU platforms in a single package. TI 15.4-Stack v2.0.1 is an evolution of the previous release, incorporating feedback that TI engineers have been diligently listening and answering here on E2E. Many issues reported have been fixed and well as optimizations in Flash and RAM consumption. Big Feature highlights include:
- Single Image Application (Changed from separate Stack and Application images in v2.0.0).
- Options to compile in/out stack features (Beacon, Non-Beacon, Frequency Hopping etc) giving HUGE flash savings.
- UART logging to visualize network/debug information without the need of the LCD Booster
Pack. - FCC and ETSI Compliance testing compile option.
- Frequency Hopping support on 863-MHz Band.
- AND MORE!!!
To download the SDK and see more information please visit http://www.ti.com/tool/simplelink-cc13x0-sdk.
The new SimpleLink CC13x0 SDK includes a migration guide to help developers easily port their existing development from TI 15.4-Stack v2.0.0 to v2.0.1.
~Brocklobsta