About RF performance test, RX sensitivity and BER curve of CC1101DK433, the RX dynamic range is from 0dBm to -95dbm (BER cretiria is 5 % ),@ 403MHz,GFSK,76 KBaud;Unfortunately, when the RSSI = -76dBm,BER is worse , up to 12%.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
About RF performance test, RX sensitivity and BER curve of CC1101DK433, the RX dynamic range is from 0dBm to -95dbm (BER cretiria is 5 % ),@ 403MHz,GFSK,76 KBaud;Unfortunately, when the RSSI = -76dBm,BER is worse , up to 12%.
Sorry about the delayed response.
The optimized setting are those you get from SmartRF Studio (see below). Simply change the RF to the desired values.
Not sure what HW you are using for testing, but I would expect the sensitivity (1% PER with 20 byte payload) to be about -100 dBm using these settings