Hi,
I was testing a application which manipules the internal flash.
Sudenly, I couldn't connect to the CC1310 Launchpad anymore.
I get this error when I trying to connect using SmartRF:
And I get this error when trying to connect using Code Composer Studio:
I already tried to re-install the XDS110 using this steps:
If manual updating or diagnostics is required, using a Windows host is highly recommended. Close any instances of CCS that are running in your system. Open a Windows Command Prompt and issue the following commands:
- Go to the directory where the utility is installed:
- C:\>cd C:\ti\ccsv6\ccs_base\common\uscif\xds110
- Run the configuration just to make sure a XDS110-class debugger is connected (or to list how many are connected) and what is the firmware revision installed on it:
- C:\ti\ccsv6\ccs_base\common\uscif\xds110>xdsdfu -e
- Put the XDS110 in DFU mode:
- C:\ti\ccsv6\ccs_base\common\uscif\xds110>xdsdfu -m
- Run the updater, passing the firmware file and resetting the debug probe afterwards:
- C:\ti\ccsv6\ccs_base\common\uscif\xds110>xdsdfu -f firmware.bin -r
But the problem remains.
What can I do?