I have installed simplelink_cc13x0_sdk_1_00_00_13 and use the ti 15.4 stack example ran on two SmartRF06 evaluation boards, one as collector and the other one as sensor.I have been stuck in such problems for a long time and very appreciate for someone's guidance:
1. Why sensor always need to receive an ACK that the transmit procedure be considered success? My sensor always retry to associate the network after transmit 6 packets(3 sucess, 3 failed with ApiMac_status_noAck).
2.Why collector cannot receive data and process a MAC_MCPS_DATA_IND event and then transmit the ACK to sensor after receive 2 or 3 packets and process them succesufl?
3.Why sensor need a long time (about 5minutes) to associate the network successful from while it is in orphan state?