I am trying to port an example to custom hardware, but I've noticed that when I do this I get a problem that effectively halts the whole application.
When EasyLink_init() is first called, the function will get all the way to here:
//Set the frequency RF_runCmd(rfHandle, (RF_Op*)&EasyLink_cmdFs, RF_PriorityNormal, 0, //asyncCmdCallback, EASYLINK_RF_EVENT_MASK);
where it then hangs. I can't see what's happening inside that function since it seems to be extern'd to somewhere else.
What's strange is this does not happen on the CC1310 LaunchPad. The only changes I have made are to the pin configuration, so I have no idea what might be causing this. Any suggestions?