Other Parts Discussed in Thread: CC110L, , CC1101, CC1350, TEST2, CC1050
Hello,
customer would like to test CC1310 Launchpad as RX with and CC110L as TX in 2-fsk modulation using below settings in smart rf studio:
// Deviation = 31.738281
// Base frequency = 434.047974
// Carrier frequency = 434.047974
// Modulated = true
// Modulation format = 2-FSK
// Manchester enable = true
// Sync word qualifier mode = 16/16 sync word bits detected
// Preamble count = 8
// Channel spacing = 199.951172
// Carrier frequency = 434.047974
// Data rate = 20.8282
// RX filter BW = 101.562500
// Data format = Normal mode
// CRC enable = true
// Device address = 0
// Address config = No address check
// CRC autoflush = false
// PA ramping = true// TX power = 10
Is it possible to set above mentioned rf parameters.
Regards, Holger