Other Parts Discussed in Thread: UNIFLASH
Tool/software: Code Composer Studio
Hi Support,
my customer is benchmarking programming SW tools to be used with XDS110 in order to program CC1310 in production.
They have found that there are more than one PC application dedicated for flashing with XDS110. They tried Uniflash (24s), DSLite (48s) and SmartRF Flash (10s) (gui and cmd line version) to program full flash of CC1310F128 with non-0xFF data.
You can see huge difference in time to do it in the brackets. I would like to ask you for help with optimal setup of DSLite tool for faster flashing. SmartRF is good enough but it can be used only for RF processors such as CC1310. They would like to use one SW for all TI chips in ideal case. The DSLite seems to be the one but it is very very slow.
You can see in enclosure our settings and the bin file to flash.
Thanks,
Alberto