Tool/software: Code Composer Studio
Try to Run "rfEasyLinkTx_CC1310DK_7xD" on own HW with CC1310F128 - (With XDS200 )
Build and Download is working.
But if I debug the Code the PIN_init () is failing ...?
When I step in the Driver file PinCC26xx.c i found following differents.
**********************
if (ChipInfo_GetChipFamily()==FAMILY_CC13x0 && ChipInfo_GetPackageType()==PACKAGE_7x7) {
// CC13xx 7x7 QFN does not have IO #0
bmReservedPins |= (1<<0);
}
*********************
don't set bmReservedPins = 1 even when the if was true ? when I debug the CC1310DK this get one Why ?
*********************
// Get number of pins available on device (from HW register)
PIN_NumPins = PINCC26XX_getPinCount();
********************
This function delivers on my board PIN_numPins = 10 and the CC1310DK 31;
Do any one have a hint what I need to change to make it happen ?