Other Parts Discussed in Thread: CC1310, CC1200, CC1201
Hi,
Our customer's CC1120 based application is into ARIB regulation test.
But they are getting spurious with the CC1120 920MHz transmitter, hence fails the Test.
As per the regulation the Permissible Values of Unwanted Emission
for 710MHz to 900MHz should be -55dBM, but the spurious with CC1120
is -50dBm (5 dBm above the regulation).
Even the TI EM boards seems to have the same result .
This design is based on the EM boards.
If possible please let us know what could be the reason for this.
Actually CC1310 based application has passed the tests without problem.
Best Regards
Kummi