Other Parts Discussed in Thread: CC110L, SIMPLICITI, MSP-EXP430FR4133, ENERGIA
Hi.
I am experiencing problems with my wireless devices, which are using CC1101 modules to communicate in 868 MHz band.
I hope, that somebody can help me find a solution. Thank you in advance.
For testing purposes I use two devices, which exchange simple messages (ping-pong) to check wireless range and stability.
The main issue is very short range - I can't get more than about 30 m LoS using external whip antenna with 3 dBi gain, cca 1 m above ground. I am using register settings generated from SmartRF studio: GFSK, 4.8 kBaud/s optimized for sensitivity.
I measured RSSI and LQI during the test. When the devices are close (cca 50 cm) I am getting RSSI -22 dB, LQI 47. When I increase distance (to cca 30 m) RSSI drops linearly to cca -80 dB, LQI stays at 47-50. When I increase the distance (to about 40 m) the communication is very unstable - only sometimes I receive packets, RSSI is about -85 dB. I am not receiving packets with lower RSSI.
Range measurements were performed on multiple places (environments), including large field, where no interference was expected.
I expect, that the range should be significantly better - about 300 m. Also the receiver sensitivity is very strange - CC1101 chip should go under -100 dB RSSI. However the weakest packets have RSSI -85 dB.
Why is LQI almost the same all the time? Is it normal? Shouldn't the LQI be much lower, when there is no expected interference?
At first I was using CC1101 modules from Aliexpress, I tried multiple antennas with similar results. Than I bought Anaren modules (Booster packs from TI Store) with onboard Antenna - I got similar results, of course I couldn't use LQI (it is not supported on CC110L).
Do you have any ideas, where could be the problem? I can perform another tests to get you more information.
Thank you.