Other Parts Discussed in Thread: CC1125, , CC1101
What is the comparable difference in receive sensitivity between CC1200 and CC1125 in 4-FSK applications from 10-50Kbps assuming minimum CHF and best modulation index for given rates?
The LNA gain looks the same. I’m aware of the narrower CHF in the 1125 but I don’t think it applies for my rates. The blocking and selectivity look slightly better in cases where the CHF is extremely narrow. Not sure about NF or other factors that may contribute to 1125 having better sensitivity but the 1125 specs list “Mobile Radio” in the list of applications and CC1200 does not. This makes me think there might be some RX performance advantages in using CC1125 that I am not yet aware of.
Looking at the spec sheets for both 1200 and 1125, the sensitivity specs around the rates I am using are not shown specifically enough for me to make an informed decision.
Example from spec sheets:
CC1200: –122 dBm 1.2 kbps 2-FSK, DEV=4 kHz CHF=11 kHz
CC1125: –123 dBm 1.2 kbps, DEV=20 kHz CHF=50 kHz
[This lead me to think the CC1125 could have some significant RX performance advantages at rates higher than 1.2 while using a wider CHF]
My application is a NLOS mobile environment with lots of multipath/fading.
As an example:
I’m currently testing using two TXREB and CC1200em (one TX and one RX) at 902-928Mhz with cable and attenuator calibrated to within 1db. On the bench the CC1200 sensitivity checks out as follows:
Mod=4-FSK, Data Rate = 10Kbps, Deviation = 4K, CHF= 16.5Khz, FEC(CC1101), whitening, PN, Viterbi:
Usable RX sensitivity (ber ~3%) = -114dbm
1. I would like to know how the CC1125 would perform with the parameters above (minus FEC which I can code into the MCU if I decide to use the CC1125).
2. Is there a performance breakdown between CC1200 and CC1125 for 4-FSK with data rates from 10-50Kbps other than those on the respective spec sheets?
3. What are the recommended parameters or register settings for optimum RX sensitivity at 10,20,30,40, and 50Kbps for the CC1200 and CC1125?
4. Besides a range extender or lowering the data rate, what other settings and techniques can be implemented to raise sensitivity and or mitigate multipath/fading?
5. Is the SMA-LNA pin loss on the CC1200em significant (>1db)?