Other Parts Discussed in Thread: CC1350
Tool/software: TI-RTOS
I want to run the simple_peripheral_cc1350lp example from here C:\ti\simplelink_cc13x0_sdk_1_30_00_06\examples\rtos\CC1350_LAUNCHXL\blestack\simple_peripheral\tirtos\ccs.
I take the simple_peripheral_cc1350lp_app_FlashROM example and open it include its stack in my workspace. I compile both stack and then the project and also run first the stack and then teh project itself. They both execute no errors. Then I lunch the project and try to run it. But when I get to
/* Initialize ICall module */
ICall_init();
It fail and run endless in assembler code.
1. Why it is append (I also try to run the project with external OAD same crush)?
2. I want to run it on the IAR. But from the information center I can't find this example. When I go to its location in the ti folder blestack examples I can open it, and compile, but I want to move it to my workspace to make some changes. Because I can't automatic open it via the example option I don't know how to move it to my workspace so it will open as expected (2 projects stack & main). Is there a user guide explain how to do it manually?